Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is my Schneider OffGrid Portable Power Station's output turning off after some time?

Issue:

Why is my Schneider OffGrid Portable Power Station's output turning off after some time?

Product Line:

Schneider OffGrid Portable Power Station

Environment:

All models and serial numbers

Resolution:

Please refer to the parameters below that are set to the PPS.

  • The AC output sockets will automatically turn off after 10 hours if the connected load is < 5W
  • The AC output sockets will automatically turn off when the battery level is < 5%
  • The USB-A and USB-C ports will automatically turn off after 10 hours if the connected load is < 1W
  • The car ports will automatically turn off after 10 hours if the connected load is < 1W

Note: These parameters are fixed and cannot be changed.

Should you have further concerns, please reach out to your local Customer Care Center at https://www.se.com/ww/en/work/support/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre