Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Upload New User Packages and Manage Roles on SAGE RTU

Issue:

Need to add, update, or delete user accounts and assign roles for secure access to RTU functions.

Product:

SAGE Remote Terminal Unit (RTU)

All Models

Environment:

  • Firmware version C3414-500-S02YZ or later
  • User Manager utility installed on PC
  • Access to RTU web GUI with Up/Download privileges

Cause:

Default user credentials (Admin/Telvent1!) are insecure and must be replaced. Role-based access control ensures compliance and limits unauthorized actions.

Resolution:

  1. Create User Package with User Manager:

    • Launch User_Manager_YZ.exe from firmware update package.
    • Add users:
      • Username: ≥5 characters, no special characters
      • Password: ≥8 characters, includes uppercase, lowercase, number, punctuation
    • Assign Role (Config, Display, Command, Up/Download, File Transfer, Remote Shell, IED Tunnel).
    • Optionally attach SSH public key (.pk2) for secure services.
    • Click Generate to create:
      • <DESC>_<VER>_Users.tar.gz (upload file)
      • access_<DESC>_<VER>.cfg (backup/recovery file)
  2. Upload User Package to RTU:

    • Log in to RTU web GUI with Up/Download privilege.
    • Navigate to Up/Download → Update Users.
    • Click Choose File, select .tar.gz package, then Send to RTU.
    • Changes apply immediately; no reboot required.
  3. Manage Roles and Sessions:

    • Max 5 concurrent logins; session timeout configurable (default 15 min, max 180 min).
    • Proper logout required to avoid lingering sessions.
  4. Password Recovery:

    • Import access_<DESC>_<VER>.cfg in User Manager if password not concealed.
    • Concealed passwords cannot be recovered.