Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Reserved Words Compilation Error/Warning

Issue

After compiling the project, I have a compilation error W1048 - Reserved Words.

Product Line

Power Scada Operation 2020

Power Scada Operation 2020 R2

Power Scada Operation 2021

Ecostruxure Power Operation 2022

Ecostruxure Power Operation 2024

Environment

Power Operation Studio Compiler

Cause

There are certain words that are restricted for use. You can find these words in the AVEVA Plant Scada manual. Reserved Words may be different version to version. Some reserved words like "Array" or "While" may result in a compiler warning. Other reserved word errors may end up causing functions to fail.

Using reserved words should be avoided as much as possible.

Schneider Electric Power Operation Version

AVEVA Plant SCADA Version

PO 2024

8.5

PO 2022

8.4

PO 2021 R1

8.3

PSO 2020 R2

8.21

PSO 2020

8.2

PSO 9.0

8.10.0.2086

PSE 8.2

8.0.0.2065

PSE 8.1

7.50.0.4150

PSE 8.0 SR1

7.50.0.4107

PSE 8.0

7.40.1.239

PSE 7.40 SR1

7.40.1.239

PSE 7.40

7.40.1.239

PSE 7.30 SR1

7.30.0.601, 7.30.1.94

PSE 7.20 SR1

7.20.4.38

PSE 7.20

7.20.1.33

Resolution

Changing the name of tags, variables or equipment in the database may result in unattended consequences and errors that are difficult to trace. Please do not attempt if you are not comfortable with Power Operation/Power SCADA or Plant SCADA. If you are using TGML graphics please call into Technical Support to consult before making attempting the changes below.

  1. Back up project.
  2. Back up citect.ini file.
  3. If there is a secondary server or virtual environment, restore the project to the secondary server under a different name and work on the changes there.
  4. Navigate to the compiler warning or error. Click on the warning.
  5. Note the current name.
  6. Rename the offending string to a word not in the Reserved Words list.
  7. Note the changes made and save the project.
  8. Navigate to the Graphics Builder. Select Tools -> Updated Pages in Active and Included Projects.
  9. Graphics Builder -> Tools -> Pack with Active and Included Pages.
  10. Power Operation Studio -> Project -> Pack with included projects.
  11. Run the compiler.
  12. Verify the warning has been removed for the line changed.
  13. Run the project.
  14. Verify correct startup of Runtime Manager services (IO Server, Alarm Server, Trend Server, etc).
  15. Verify alarming is functional.
  16. Verify communications and graphic functionality including one line.
  17. Verify trending functionality.
  18. Verify any custom utilities.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre