Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the wireless switch set pre-paired, or does the customer need to pair it manually?

The XB5RFB01, XB4RFB01 and XB5RMB03 are packs with non-programmable receivers.

That means these packs come with button already paired with receiver in factory and it is not possible to change, remove or add any other button.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: