Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does EcoStruxure Control Expert v16.2 use the predefined custom path by default ?

1. Issue

Starting from Control Expert v16.2, the predefined custom path is used for operations such as Open, Save and Export, because the “Use defined custom path” option is enabled by default.
This feature, available under Tools → Options → Paths, was introduced to ensure consistency and prevent accidental saves in unintended directories.
In previous versions (16.0 and 15.x), this option was not functioning as intended, and the software always used the last opened path instead.

2. Product Line

EcoStruxure Control Expert v16.2.

3. Resolution

To restore the previous behavior (using the last opened path):

  • Go to Tools → Options → Paths.
  • Uncheck “Use defined custom path.”

Keeping the option checked ensures the software always uses the predefined custom path.

Use defined custom path

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre