Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use an input to run or stop a M580 hot standby controller?

Issue

Use an input to start or stop PLC


Environment

Control Expert


Product

M580 HSBY


Resolution

This is not available on hot-standby controllers. Only available on standalone.