Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is any action needed before updating M580 Firmware to version 4.01 or later?

Updating from firmware version 3.20 or earlier to firmware version 4.01 or later must be done following a two-steps specific procedure. For instructions, refer to the M580 Firmware Installation Guide.

Besides, thanks for following the next recommendations if intended to upgrade the M580 controller with a firmware version 4.01 or later, as explained in Firmware History Release Notes RN0000000110.03 :

  1. In case you are using a Modicon M580 RTU module in association, first upgrade the RTU module to firmware version 03.02.02 or later and test your application.
  2. In case you are using a Modicon BMENOC0301 or BMENOC0311 module in association, first upgrade the BMENOC module to firmware version 02.20 or later and test your application.
  3. In case you are using a Modicon BMENOC0321 module in association, first upgrade the BMENOC module to firmware version 1.09 or later and test your application.