Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to online Install a Brand-New M580 CPU in a hot standby system

When installing a brand-new CPU during the production operation of the system,

-do not connect the network cable between the master and standby CPUs.

After the CPU and CRA are all fully operational, connect the network cable to construct the ring network.

-Alternatively, in accordance with the operating procedure outlined in the user manual,

you can first download the program to the brand-new CPU independently, then integrate the CPU into the on-site control system.

Control Expert manual capture

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre