Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to solve EcoStruxure Control Expert Assent Link 4.0 installation error?

Issue

EcoStruxure Control Expert Asset Link Installation fails, causing ERROR 1603, if the License Manager/Floating License Manager version is greater than 2.9

Product Line

EcoStruxure Control Expert - Asset Link

Resolution

Install EcoStruxure Control Expert Asset Link 4.0 SP1, which mitigates the lack of compatibility with License Manager/Floating License Manager version greater than 2.9.