Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Edge Firmware Visibility and Version Verification

When the edge firmware is updated prior to updating the RTU firmware, the edge firmware may not be displayed in Remote Connect.

To verify the edge firmware version:

  1. Establish an SSH connection to the device using PuTTY.

SSH using putty

2. Enter the following command "verinfo"

verinfo

This will give the edge firmware version.