Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What could cause a M580 safety PLC safe task to come up in STOP mode after a power cycle?

Issue:

possible cause of M580 safety PLC safe task to come up in STOP mode after a power cycle


Product Line:

M580 Safety PLC, Ecostruxure Control Expert


Resolution:

One possible cause of the safety Task to come up in STOP mode is if the  "support quantum remote drops" option in the processor configuration is selected and there is no Quantum drop configured in the projectimage1

Uncheck the "Support Quantum Remote drops" option in the processor configuration. This is would be an offline change and thus require a project download to the PLC.

image2

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: