Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How the "broken wire" option on X80 analog input modules works?

Issue:

How to use the "broken wire "option embedde in X80 analog module ? (Example using BMXART0814 analog input module ).

Product Line:

X80 analog modules with "broken wire" option available

Environment:

EcoStruxure Control Expert, Windows 10

Resolution:

Example using the BMXART0814 analog input module with the 'Broken Wire Test' enabled:

capture 1

If one of the input wires becomes broken or disconnected, the fault can be detected using one of the following methods:

  • The module's 'ERR' LED will turn red, and the corresponding channel LED will blink to indicate the fault:

cap

  • The faulty channel will be displayed in the Debug view of the module:

Capture 1

  • If the "READ_STS" FFB is used in the plc program, It will provide more details on the IODDT:

  • Capture 2

Using with the T_ANA_IN_T_BMX device DDT configured:

Capture 3

Using the T_U_ANA_TEMP_IN_8 device DDT configured:

Capture 4

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: