Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Installing OPC UA on SCADAPack via Node-RED

Prerequisites

Before proceeding, review the article:
“SCADAPack 47xi Application Note – Docker App Connectivity and Redis Overview”
Link: https://www.se.com/in/en/download/document/SCADAPack47xiDockerAppConnect/


Installing OPC UA on SCADAPack using Node-RED

You can install OPC UA on SCADAPack via Node-RED using two methods:

Method 1: Update the Bundle_NodeRed.sh Script

  • Modify the SDK script Bundle_NodeRed.sh to include node-red-contrib-opcua.

Method 2: Install from Node-RED Palette

  • Requires internet connectivity on the SCADAPack Edge device.

Here, I have used two packages to demonstrate these two methods(node-red-contrib-opcua, node-red-contrib-iiot-opcua )

Method 1: Update the Bundle_NodeRed.sh Script

(No internet required on SCADAPack Edge)

  1. Locate the SDK script Bundle_NodeRed.sh on your development system.
  2. Edit the script to include the package:
    node-red-contrib-opcua

edit script

  1. Save the updated script.
  2. Deploy the modified script to the SCADAPack Edge board.
  3. Open Node-RED in a browser.
  4. Navigate to Manage Palette → Nodes.

pallette

install method1

  1. Verify that the OPC UA package is listed as installed.

validate method 1

validate 1

Method 2: Install from Node-RED Palette

(Requires internet connectivity on SCADAPack Edge)

  1. Ensure the SCADAPack Edge board has an active internet connection.
  2. Open Node-RED in a browser.
  3. Go to Manage Palette → Install.
  4. Search for:
    node-red-contrib-iiot-opcua

method 2 search

  1. Click Install and wait for completion.

install method 2

  1. Confirm the package appears under Manage Palette → Nodes.

validate method 2 1

validate method 2 2

Schneider Electric Saudi Arabia

Attachment(s)
Bundle_NodeRed.zip [6.94 KB]