Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I create a new project in EcoSet Config?

To create and design multiple switchboard, and to configure it , you must create a project. When a new project is created, you can develop multiple switchboards and configure each switchboard with required switchgears.

  1. Click Create a project.
  2. Enter your project name and update the basic information.
  3. Select the latest price list from the Applied price list drop down menu.
  4. Click Create.

Your new project is now created, and you can proceed to create a new switchboard.

The following tabs will appear in sequence.

Tabname

Function

MANAGESWITCHBOARD(A)

To manage multiple switchboards for a project.

SELECTAPRODUCT(B)

To create and manage switchboards.

SINGLE LINE DIAGRAM (C)

To generate and view the single line diagram.

DESIGN A SWITCHBOARD (D)

To select and manage switchboards.

BILLOFMATERIAL(E)

To generate bill of material for the final products.

EXPORT(F)

To export all project related documents in different document format like pdf, csv, jpg.

Manage Switchboards

new project