Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Compact DAP204 to X80 DRA0804/0815 quick wiring - 990XSM00203

Issue

Migrating an ASBDAP204 to a BMXDRA0804/0815 and need to confirm the 990XSM00203 quick wiring cable pinout.

Product line

Modicon X80, M340, M580

Resolution

Below is an image of the pinout.

pinout

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: