Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are There Any Limitations for the OPC UA Server in EcoStruxure Operator Terminal Expert?

Article available in these languages: Spanish

Issue:

Is there any limitation for the OPC UA Server with Operator Terminal Expert?

Product:

EcoStruxure Operator Terminal Expert v3.x , v4.x (EOTE)

Environment:

HMI Configuration Software in Windows

Resolution:

There is no strict limit; however, monitoring a large number of variables can impact HMI performance.

The recommendation from R&D is to keep OPC UA communication variables below 5,000 (this number was validated by R&D in previous tests).