Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Nutanix Files Start fails if sufficient time is not allowed after cluster is started.

Issue:

Nutanix Files Start command fails when issued shortly after cluster startup completes.

The following message appears in the error.log file -

2025-12-10T01:07:15,435 ERROR Thread-32 com.apcc.pcns.nutanixservice.NutanixSshConnection - startAfs() - AFS start command failed with result ERROR: Unable to power on vms for fileserver

2025-12-10T01:07:15,435 ERROR pool-9-thread-1 com.apcc.m11.components.shutdowner.NutanixClusterOps java.util.concurrent.ExecutionException: java.rmi.RemoteException: Failed to start AFS
at java.base/java.util.concurrent.CompletableFuture.reportGet(CompletableFuture.java:396) - startAFS() - failed to start AFS: {}

Product:

PowerChute Network Shutdown version 5.2

Environment:

Nutanix AHV 10.3, AOS 7.3

Cause:

The Files Start command fails when issued shortly after the cluster startup completes.

Solution:

Increase Cluster Start duration to allow enough time between cluster start and attempt to re-start Nutanix Files. This may need to be set between 10 and 15 minutes.