Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to create Mold Case Circuit Breaker (MCCB) Compact NS part no.
Please be informed that part no. of  Mold Case Circuit Breaker (MCCB) Compact NS is created by 10 digit.
So customer has to know some main characteristic of MCCB as list below
- Frame rating
- Breaking Capacity type
- Number of pole
- Fix/Drawout
- Micrologic trip unit protections
- Charging Motor
- Power connection
For more information and clarification, kindly find attach table for selection and example.

However, the individual datasheet is not available for Compact NS.
Therefore the characteristic, connection, dimension and ETC, kindly refer to Global Catalog as attachment.

การเลือกรหัสสินค้าสำหรับ MCCB รุ่น ComPact NS

Schneider Electric Thailand

Attachment(s)
Compact NS 2018.pdf [39.15 MB]