Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Wiring for NSX100 to 630A 4P circuit breaker
In the 4P configuration of MCCB, you can connect the neutral & one phase in case of single phase application.
See a wiring diagram for NSX 100 ..630 Amps as attached. Although the attached diagrams are for 3P MCCB, you can use the same wirings by connecting the the neutral & one phase and leave the inner two poles blank of single phase application.

Schneider Electric Thailand

Attachment(s)
Compact NSX wiring.pdf [189.44 KB]