Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power supply (control power) for EasyLogic (PM2110/PM2120/PM2130)
For the power supply, please see the diagram and information below.
picture : power supply, please see the diagram and information

250 mA fuses= 250 mA fuses

L1 and L2 are non-polarized. If using an AC power supply with neutral, connect neutral to the meter’s L2 terminal.
Always use a fuse on L1. Fuse L2 when connecting an ungrounded neutral to the control power.
If using a control power transformer, fuse both primary and secondary sides of the transformer.
The fuses / circuit breakers must be rated for the installation voltage and sized for the available fault current.

Schneider Electric Thailand