Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
APC AVR - Automatic Voltage Regulator Equipment

APC AVR - Automatic Voltage Regulator Equipment is Line R series.

The Line-R automatically corrects brownouts (by boosting low voltage) and overvoltages (by stepping down high voltage) from the power utility service to levels that are safe for computers, as well as other sensitive equipment. APC by Schneider Electric’s Line-R provides the highest degree of protection from line voltage sags and swells, and has been designed for many years of reliable, maintenance-free service.

The Line-R is designed for use with voltage sensitive equipment such as a: computer, monitor, inkjet printer, scanner or fax. It is also designed for use with home electronics (TVs, stereos, CD players, etc.).

Photo1

Schneider Electric Thailand

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: