Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Setting up the screen passwords for EasyLogic PM2200 series?
It is recommended that you change the default password in order to prevent unauthorized personnel from accessing password-protected screens such as the
diagnostics and reset screens. This can only be configured through the front panel. The factory-default setting for all passwords is “0” (zero).

1. Navigate to Maint > Setup.
2. Enter the setup password (default is “0”), then press OK.
3. Navigate to HMI > Pass.
4. Move the cursor to point to the parameter you want to modify, then press Edit.

1

5. Modify the parameter as required, then press OK.
6. Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
7. Press the up arrow to exit.
8. Press Yes to save your changes.

Schneider Electric Thailand