Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to select busbar to install at masterpact NW?
We recommend to select the busbar sizing and the amount of busbar as the table as attached.

For example

masterpact NW?

Solution:
For Ti = 50 °C, use an NW40 which can be connected with five 100 x 10 mm bars.

Schneider Electric Thailand

Attachment(s)
Busbar sizing table.pdf [339.31 KB]