Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the problem when the heartbeat LED of PM2100 flashing?
heartbeat / serial communications LED is the LED indicators alert or inform you of meter activity

What is the problem when the heartbeat LED of PM2100 flashing?

Troubleshooting LED indicators

Abnormal heartbeat / serial communications LED behavior could mean potential problems with the meter.

What is the problem when the heartbeat LED of PM2100 flashing?

If the problem is not fixed after troubleshooting, contact Technical Support for help and ensure you have your meter’s firmware version, model and serial number information available.

Schneider Electric Thailand