Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the application types of each Masterpact NW performance levels
Masterpact NW have 5 performance levels

N1 - for standard applications with low short-circuit levels.
H1 - for industrial sites with high short-circuit levels or installations with two parallel-connected transformers.
H2 - high-performance for heavy industry where very high short-circuits can occur.
H3 - for incoming devices supplying critical applications requiring both high performance and a high level of discrimination.
L1 - for high current-limiting capability and a discrimination level (37 kA) as yet unequalled by any other circuit breaker of its type; intended for the protection of cable-type feeders or to raise the performance level of a switchboard when the transformer power rating is increased.

Schneider Electric Thailand

Attachment(s)
NW performances.pdf [239.2 KB]