Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is a heat loss of MV Switchgear F400?
The heat-power that dissipate from the different cubicles.
Characteristics ot typeValues
Insulation level170170185
KV, 1,2/50µs impulse
Rated normal current (A)125025001250
Type of circuit breakerSF1SF2SF2SF1SF2
The heat-power that dissipate (W)5605601530560560

Schneider Electric Thailand