Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Installation Instruction of SpaceLogic Thermostat TC900 Series for Digital Fan Coil Applications
The TC900 Series fan coil thermostats are optimized for office building, hotel, hospital and residential applications. The TC900 Series can be used for 2-pipe or 4-pipe applications.

Available in two housing finishes: optimum (black glass display with capacitive buttons on a white base) or medium (white glass display with mechanical buttons on a white base).

The TC900 Series is both easy to operate and install. The devices feature microprocessor-based control and large backlit LCD screens which display operation status (cooling, heating, and ventilation), fan speed, room temperature and set-point.

Please find Installation Instruction as attached.

Schneider Electric Thailand

Attachment(s)
TC900 Series Digital Fan Coil Thermostat Installation Sheet.pdf [1.03 MB]