Size bugün nasıl yardımcı olabiliriz?

How do I install Vijeo Designer Application onto a New Magelis running Windows and Vijeo Designer Runtime from USB Stick

Issue:

How do I install Vijeo Designer Application onto a New Magelis running Windows and Vijeo Designer Runtime from USB Stick

Product Line:

Vijeo Designer, Magelis, Harmony

Resolution:

Make sure you are using a quality USB stick
Vijeo Designer and the Vijeo Designer Runtime must be matching revisions
Format the USB stick - FAT32

In Vijeo Designer - Navigator - Select your target
with the Property Inspector - Select Download - Click the + to expand - Change Download to File System - Change Path to the Drive location of the USB stick

Right click your target - Select Download to (File System)...
[The Project must be saved in order to download a backup to the target. Save project and continue download] Select Yes
After Downloading Complete
Safely Remove USB Mass Storage Device
Remove USB Stick

Install USB Stick on Magelis
Select Start -> All Programs->Schneider Electric->Vijeo Designer->Tools->Vijeo Designer Application Installer
Browse for the .VDA file on the USB Stick
Open
After it is complete

Select Start ->all programs->Schneider Electrci->Vijeo Designer->Vijeo Designer Runtime

Your Application should start running.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)