What are the baud rate options on the ATS48 modbus port?
Needs to know the baud rate for ATS48 modbus
Product Line:
ATS48
Environment:
All
Cause:
Need to use 115.2 baud
Resolution:
ATS48 modbus is only available at 19200 or 9600.
Please note that the remote HMI only works with the 19200 baud rate.