我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the ohmic value and average power for the resistor used in the VW3A66713 dynamic brake kit?
Issue:
Ohmic and power value for resistor used in the VW3A66713 dynamic brake kit

Product Line:
Altivar Drives

Environment:
All

Cause:
NA

Resolution:
The value is  of the resistor is 28 ohms and the power is 204 watts.