我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the Altistart 48 require separate control power?
Issue:
Does the ATS48 require separate control power?

Product Line:
ATS48

Environment:
All

Resolution:
Yes, terminals CL1 and CL2 require 90 to 270 Vac, 50/60 Hz to supply control power.
It is common to use 120 VAC to supply power for the ATS48 control power.