我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the VA consumption of CL1, CL2 control power on an ATS48?
Issue:
VA consumption of CL1, CL2 control power on an ATS48

Product Line:
Altistart 48, ATS48

Environment:
All models, All serial numbers.

Cause:
Need to know the power consumption.

Resolution:
ATS48D17Y and ATS48D22Y require 25 Watts.
ATS48D32Y, ATS48D38Y, ATS48D47Y, ATS48D62Y, ATS48D75Y, ATS48D88Y, ATS48C11Y, ATS48C14Y, and ATS48C17Y require 30 Watts.
ATS48C21Y, ATS48C25Y, and ATS48C32Y require 50 Watts
ATS48C41Y, ATS48C48Y, ATS48C59Y, ATS48C66Y, ATS48C79Y, ATS48M10Y and ATS48M12Y require 80 Watts.

Data from Table 31 (page 83) of document S1A37491: Altistart 48 Y-Range Soft Start Controllers Instruction Bulletin