我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are the ATS48 soft starters available in a NEMA 3R enclosure rating?
Issue :
Looking for an ATS48 installed inside a NEMA 3R enclosure.

Product Line :
Enclosed 48

Environment :
All

Cause :
Enclosures for the ATS48

Resolution :
Yes. Nema 3R is available in the Enclosed ATS48 packages.
See the attached document.


施耐德電機Taiwan

附件
8800BR0402.pdf [497.89 KB]