我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the contact ratings of 9001KA contact blocks?
Issue:
Contact ratings of 9001KA contact blocks

Product Line:
30mm Pushbutton

Environment:
9001K/SK/KX 30mm Push Buttons

Cause:
Confirm the rating of the contact block for an application.

Resolution:
The 9001 KA contacts are rated NEMA A600. The maximum AC voltage is 600VAC and the maximum thermal current is 10 amps.
9001 KA contacts are also rated NEMA Q600. The maximum DC voltage is 600VDC and the maximum thermal current is 2.5 amps.