我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the part number for the latch bar rivets for the Class 9423 Type M door closing mechanisms?
Issue:
Latch Bar Rivets for the Class 9423M3, M4, M9, M23 and M24.

Product Line:
Operating Mechanisms,Disconnect Switches, and Door-Closing Mechanisms

Environment:
9423 Door-Closing Mechanisms

Resolution:
The door closing mechanisms are supplied with the 31008-124-01 rivet(s) as standard. For replacement purposes order as outlined below:

9423M3 and 9423M23; requires (1) 31008-124-01 rivet.
9423M4, 9423M9 & 9423M24; requires (2) 31008-124-01 rivets.