我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are barrier kits available for the 9422ATF11, 9422ATF12 or 9422ATF13 200A or 9422TG 400A switches?
Issue:
Do we have fingersafe covers for the 9422ATF11, 9422ATF12, 9422ATF13 or 9422TG Operating mechanisms?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
9422 Disconnect Switches

Resolution:
No. Barriers are currently only available up to the 100A mechanism, 9422TE.