我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What does the T indicate in the LC1DT contactor catalog number?
Issue:
LC1DT catalog numbers

Product Line:
IEC Contactors and Starter

Environment:
Tesys D line Contactors

Resolution:
The T indicates that the device is a 4 poles with all normally open poles.  4 pole units only have resistive (AC-1) power contact ratings.