我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?
Issue:
Is a TVSS unit catalog number TVS4EMA16A compliant with specification UL1449 3rd edition?

Product Line:
TVSS.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, a TVSS unit TVS4EMA16A has a UL1449 3rd edition listing, and has an identification sticker on the inside of the unit that indicates this.
NOTE: The TVS4EMA16A is obsolete and replaced by the SSP04EMA16 (in a NEMA 1 enclosure or SSP04EMA16S in a NEMA 4 SS enclosure) and the SSP04EMA16 is UL1449 5th edition listed.


CTA-ID : 2053576

施耐德電機Taiwan

探索更多
產品:
探索更多
產品: