我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does Schneider offer a soft start for a single phase motor?
Issue:
Soft start for a single phase motor?

Product Line:
ATS01

Environment:
All

Cause:
Needs a soft starter for a single phase motor.

Resolution:
Yes, but the offering is limited.  The ATS01N1**FT products are rated for single phase motors up to 2HP at 240V and 1/2HP at 120V.
See the attachment beginning on page 34.  Reference page 40 for part number selection.

施耐德電機Taiwan

附件
8637CT0401R12_11.pdf [2.61 MB]