我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Does the ATS01 come with a shorting contactor?
Issue:
Does the ATS01 have an internal shorting contactor?

Product Line:
Altistat 01

Environment:
All

Cause:
N/A

Resolution:
All of the ALTISTART 01 models, except the ATS01N103FT and ATS01N106FT, have an internal shorting contactor as standard.