我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Why do I not see the check box for "Command File" in PowerChute Business Edition when viewing the interface using Firefox?
Issue:
Viewing PowerChute Business Edition interface using Firefox and the Command File check boxes are missing.
firefox screenshot with check box
Firefox screenshot without check box


Product Line:
PowerChute Business Edition (PCBE)

Environment:
Firefox web browser versions 25 and older

Cause:
Undetermined

Resolution:
We recommend updating to the latest version of Firefox.

With older version of Firefox mouse over the area where the check box should be and click. The check boxes will appear.