我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the maximum equipment & cable mounting depth for the NetShelter WX?
Issue:
Will deep IT gear fit into the NetShelter WX, and if so, how much clearance will remain for cabling?

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
The NetShelter WX is shallow which can make installation of deep rack gear challenging.

Resolution:
Please see attached file

施耐德電機Taiwan

附件
20130918 Maximum Equipment Mounting Depth for a NetShelter WX.pdf [322.12 KB]