我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Are the NetShelter CX and CX Mini delivered fully assembled?
Issue:
Need to know if the NetShelter CX and Mini arrive assembled.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Customers may ask if assembly is required.

Resolution:
The NetShelter CX Mini arrives on its castors with the brush strip attached to the underside, on a pallet, and the keys inside.
The NetShelter CX arrives on a pallet with ramps supplied. The PDU power cord, leveling feet, keys and documentation are packed separately inside the cabinet.