我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What options are there for an ATS48 Soft Start to communicate via Modbus Ethernet?
Issue:
ATS48 communication options via Modbus Ethernet.

Product Line:
Altistart  ATS48

Environment:
All

Cause:
Communications Options

Resolutions:
The softstart has built-in Modbus RTU.
Consider a Modbus to Ethernet Gateway such as the EGX150.