我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Is there an Ethernet TCP/IP option on the ATS22 Soft Starter?

Issue:
Does Schneider Electric offer a Modbus RTU to Modbus Ethernet TCP option on the ATS22 Soft Starter.

Product Line:
Altistart ATS22

Environment:
All

Cause:
Ethernet option on the ATS22 Soft Starter

Resolution:
The Soft Starter has a built-in Modbus port. A Modbus-to-Ethernet Gateway (EGX100SD) can be used to interface between Modbus and Ethernet communication. Gateway

施耐德電機Taiwan

附件
Class 9998 and 9999 Control Accessories_EGX100SD Ethernet Gateway.pdf [80.39 KB]