我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Which fiber port in an NMS25102 switch is TX

Issue
The fiber optic ports in this switch are unlabeled. Which is TX and which is RX?

Product Line
ConneXium switch

Environment
499NMS25102

Resolution
The upper connection is TX the lower one RX.