我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
In Vijeo Designer, how many characters can I use for the project description?

Issue:
How many characters can be used for the project description in Vijeo Designer

Product Line:
Vijeo Designer


Resolution:
The project description field allow a maximum of 255 characters.