我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
Can the Serial Communication protocol of an M340 PLC be changed dynamically?

Yes the Serial Communication can be changed dynamically from Modbus Master, Modbus Slave, or Character mode by using a WRITE_CMD (%MWr.m.c.24.bit) and toggling bits 12, 13, or 14 respectively.
Example:
1) Bit 12 = 1, bits 13 & 14 = 0 Current protocol is changed to Modbus Master
2) Bit 13 = 1, bits 12 & 14 = 0 Current protocol is changed to Modbus Slave
3) Bit 14 = 1, bits 12 & 13 = 0 Current protocol is changed to Character Mode