我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the M340 spacing requirements, when installing a backplane (BMXXBP ••••) in an enclosure?

Issue:
M340 spacing requirements, when installing a backplane


Product Line:
M340


Resolution:
When assembling BMX XBP racks certain installation rules must be complied with.
image1

image2