我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What is the maximum number of Security Groups and Users you are allowed to have in Vijeo Designer?

Issue
Maximum number of Security Groups

Product Line
Vijeo Designer

Resolution
Vijeo Designer 6.1 supports, for each target, a maximum of 20 security groups. Each security group supports a maximum of 100 users.